KM Space_User_Settings
KM Space_User_Settings
| Address: | 22918 (5986H) | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Type: | WORD | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Access: | Read/Write | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Unit: | -- | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Range: | -- | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Default Value: | -- | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Store Supported: | No | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Description: |
This object is used to activate some functionality during the application execution.
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Notes: | -- |